5/27/2018 10:28 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello WojciechP; The As-i addressing module is the easiest way of select a new the slave addresses for a module in your As-i network. Depending on your selection of As-i master, some will have functionalities to set a slave address over the network, under certain conditions. This is how this functionality is described for the CP 343-2 As-i master, for example (see attachment below), Notice that only one (new) slave with address 0 can exist on the network at a time if you can want to change its address through the CP 343-2 master Manual CP 343-2/CP 343-2P AS-Interface Master (Edition 2008) with Supplements (Edition 08/2010). https://support.industry.siemens.com/cs/ww/en/view/5581657 Hope this helps, |
This contribution was helpful to1 thankful Users |
Follow us on