6/29/2012 9:33 AM | |
Posts: 73 Rating: (2) |
As per my original post... On button press : set bit= Works ok Thanks for the suggestion though! Plazz |
6/29/2012 9:37 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Plazz, Which version of Software are you using? (including Service Packs and Updates) Best regards, Wizard |
6/29/2012 10:57 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Plazz, Ok, that is the right version. Please have a look at the following link: Updates for STEP 7 V11 SP2 and WinCC V11 SP2 please read the readme file for Update 3. Here you will find that the mentiond function isimproved. Please perform an OS update Hereis a link: how do you do an operating system update (OS update) on operator panels? Best regards, Wizard |
6/29/2012 12:21 PM | |
Posts: 73 Rating: (2) |
Thanks Wizzard but I have already performed an OS update prior to loading my program for the first time and therefore the HMI is already up to date? Plazz |
6/29/2012 1:20 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Plazz, Ok, but did you use the option "Reset to factory Settings"? If not, please perform an OS update againg, but now with option "Reset to factory settings" selected. Otherwise, I would advise to start a Service request: Support Request Best regards, Wizard |
Follow us on