4/30/2016 8:18 PM | |
Joined: 10/11/2014 Last visit: 7/11/2023 Posts: 79 Rating: (1) |
you mean i can not give an upload from panel with tia portal ? |
4/30/2016 8:19 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: How do you backup/restore with a Comfort Panel?It is not possible to open and process the backup file with WinCC (TIA Portal). The file can only be downloaded to the original or another panel of the same type with a restore procedure. Uploading the project is not possible for Comfort panels up to now. may be Siemens solve this problem in the future. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
4/30/2016 8:32 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, This option is not available for TIA Software. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
4/30/2016 8:47 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, You can use Prosave but just to take backup from the image file downloaded to the panel. This image is not editable. You can use Prosave once again to restore the same image to another Panel have same part number. Prosave is a free software and If you have any SIMATIC HMI software installed on your PC. You will found it installed as well. Here's bellow the cable needed to use with your panel and other Simatic Panels as well. Which connector cables are available for connecting to SIMATIC Panels? |
Ayman Elotaify |
|
Follow us on