5/17/2016 5:51 PM | |
Joined: 8/8/2014 Last visit: 6/14/2022 Posts: 52 Rating: (3) |
Dear colleagues, please advice - I'm a beginner with KTP1000 panel, have a project on PLC (which is Ok) , and want to add HMI panel I have there. I can make online connection, but message window says the HMI "defective" - pls see attached file. Seems that it is "OS update" issue, is not it ? May I follow this procedure ? Q2. How can I import tags from PLC part of the project (PLC now in the field, so I can not make online connection to it) into HMI part of the project ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/19/2016 1:07:00 PMNew subject after splitting |
|
Follow us on