Industry Online Support
Technical Forum
12/15/2014 7:27 AM | |
Posts: 2 Rating: (0) |
Hello I've create a new project in TIA13 using the KTP1200DP basic but running the simulator appear the layout of the panel (including function keys) with a blue screen without any designed element. I've create another project using the wizard but running the simulator the effect is the same. TIA13 is updated at Update 6 The simulator with other panels i.e. TP1500 Confort run properly. Anyone know this problem? Thanks in advance
AttachmentTest.zip (93 Downloads) |
12/15/2014 11:47 AM | |
Posts: 2 Rating: (0) |
Sure TIA is updated at Update6 and HSP is installed viceversa i cannot create the project with KTP1200DP |
Follow us on