7/13/2018 7:54 AM | |
Posts: 8 Rating: (0) |
hi all, i'm also doing the project similar to this topic, any expert can help? i'm using KTP400 Comfort panel. i have refer the read and write to csv file example, but that is not i want. what i want is, when click a button, then will display all the csv file name that inside the folder. Then user can refer to the display, and then key in the name of csv file manually. After that user will click another button, then the contain in the selected csv file will fill in to the internal tag. I want the function something like picture below, but the code in the picture is not for KTP400 comfort panel. ------------------------------------------------------------------------------------------ |
Last edited by: 5877 at: 7/13/2018 12:05:03 PMLast edited by: Jen_Moderator at: 7/13/2018 1:07:25 PMNew subject after splitting |
|
Follow us on