Industry Online Support
Technical Forum
3/31/2012 5:32 AM | |
Posts: 21 Rating: (0) |
Dear all: How can i do if i need a large of data handling in FM458? It is too long if i put it in S7-400.Thanks. |
3/31/2012 10:56 AM | |
Joined: 8/25/2006 Last visit: 4/25/2024 Posts: 2203 Rating: (277)
|
Hello. What size of data do you want to transfer to S7-CPU? Look at themanual, chapter 4.3.1, where you will find the overview of 3-type data transfer, and use the third (data sets/blocks). |
3/31/2012 5:19 PM | |
Posts: 21 Rating: (0) |
the data read from EXM438-1 analog signal. there are perhaps 7000 real data i want to save and handle in FM458 .how should i do? |
3/31/2012 6:08 PM | |
Joined: 8/25/2006 Last visit: 4/25/2024 Posts: 2203 Rating: (277)
|
Hello. You may use "Communications utility, trace" (function block TRCC) or "Pointer-based communications" (function block DB_P). You read about this in the manualSIMATIC D7-SYS Selecting Function blocks(chapters 1.4.4 and 1.4.8). |
This contribution was helpful to1 thankful Users |
4/1/2012 6:13 AM | |
Posts: 21 Rating: (0) |
Thank you. |
Follow us on