4/30/2021 10:10 AM | |
Joined: 8/2/2017 Last visit: 6/18/2024 Posts: 2 Rating: (0) |
Hello, We must move a mechanism with position control by laser distance sensor. We are going to use the position controller in SINAMICS (Basic positioner EPOS) and encoder for it will be the laser distance sensor Dimetix DAN-10-150 by SSI interface. The manual for Dimetix (chapter 3.9): https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=&cad=rja&uact=8&ved=2ahUKEwintoqgwaXwAhWjlosKHeMHCwQQFjAAegQIBBAD&url=https%3A%2F%2Fdimetix.com%2Fwp-content%2Fuploads%2F2018%2F02%2FTechnicalReferenceManual_DSeries_V103.pdf&usg=AOvVaw3RJrN-WMlMwvDuPv6IzR5A Will CU250S-2 be work with DAN-10-150? Can we use such solution? AttachmentTechnicalReferenceManual_DSeries_V103.pdf (135 Downloads) |
Last edited by: Jen_Moderator at: 04/30/2021 11:08:53Added PDF as an attachment. |
|
5/3/2021 11:50 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, the basic configuration of a SSI encoder is shown in chapter 8.22.3.4 of the CU250S-2 operating instruction manual. The basic setup of a linear laser encoder is also shown on the following application example. I haven`t used this type of encoder myself, but this is a common application on the CU250S-2 as you can see on the manuals. On the first look at the technical data of the laser encoder I don`t see any blocking points so I wouldn`t expect any issues.. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on