3/8/2009 7:38 AM | |
Posts: 557 Rating: (64) |
hi You can go to control panel of op & increase the brightness & contract. regards vivek |
3/9/2009 9:24 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello Basicly type and resolution on both LCD are the same. But I can't answer if old one can be replace by other model Model: MTG-E8619-A3 . For the old LCD, was impossible to find info in details. So my suggestion is to think for change whole panel, not only LCD. For this type of OP, life cycle is on Product discontinuation since 2008-10-01.. And if you haven't spare OP (the same type), better change it. By the way, you have already cleaned the surface of the screen inside, have you? An also increase the brightness? regards |
3/10/2009 11:53 AM | |
Posts: 20 Rating: (0) |
yep i try my all the best and service it completly but the problem is inside the LCD Might be its Life is over any ways thanks for repkly regards Usman |
Follow us on