6/11/2013 1:12 PM | |
Posts: 4 Rating: (0) |
Hello Exist commandfor automatic lead on HDD to NCand opposite? Thanks |
6/11/2013 4:12 PM | |
Posts: 391 Rating: (50)
|
I guess you mean "Load" from HDD to NC and "Unload" from NC to HDD. You can give a look at the functionality "job lists" with which you can define one or more lists of operations. In every list you can put commands to: Load/Unload a program Copy a program Select a program for execution ... The PLC program can decide when the HMI-Advanced has to execute one of these lists. The only problem is: you have to prepare these lists in advance and it is not possible to change them automatically. This is not goodfor example if the names of the programs to load/unload are always different. It works fine if the names of the programs are always the same but their contents change. More on job lists: https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SIMODRIVE_04_2010_E/BAD.pdf?p=70#page=70&view=FitBH,0&pagemode=none https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SIMODRIVE_04_2010_E/IHA.pdf?p=119#page=119&view=FitBH,0&pagemode=none |
6/18/2013 2:58 PM | |
Posts: 391 Rating: (50)
|
If the machine has HMI-Advanced as operator interface, an alternative to job lists might be: //M(Test)
|
This contribution was helpful to1 thankful Users |
6/20/2013 2:17 PM | |
Posts: 4 Rating: (0) |
hm... |