Industry Online Support
Technical Forum
3/10/2011 6:08 PM | |
Posts: 74 Rating: (3) |
Dear Tomy Master A new level radar, the Siemens Sitrans LR560 has just been released. It can domeasurements to 100m range and the temperature at the face of the radar can be as high as 200C. This radar transmitter has some unique features, allowing some creative mounting options allowing the temp at the radarto be much lower than the process. Here is the link https://www.automation.siemens.com/w1/automation-technology-sitrans-lr560-19704.htm From my perspective, your application is a bit too special to be dealt with over a forum or e-mail. I would suggest you contact a Siemens Process Instruments Specialist in your country. I might be able to help you with that if needed. Regards Toppie [ |:) |
Follow us on