2/25/2019 12:02 PM | |
Joined: 11/15/2017 Last visit: 8/13/2023 Posts: 6 Rating: (0) |
Hi, we've bought assembly 6ES7656-6CL30-1BF0: PCS 7 CPU 410 REDUNDANCY AUTOMATION SYSTEM ALREADY ASSEMBLED AND TESTED: WITH 2X CPU 410-5H PROCESS AUTOMATION INCL. AS RT PO 100; WITH 2X SYSTEM EXPANSION CARD PO 500; WITH 2X 2 10M SYNC-MODULES AND 2X 1M FO; W/O CP443-1IE; WITH 1X UR2-H (2 X 9 SLOTS) ALU RACK; WITH 2X UC 120/230V 10A POWER SUPPLY; INCL. IL-RUNTIME LICENSE BUNDLE RELEASE: F; W/O CP443-5EXT (PROFIBUS); For that PLC we've bought AS PO licenses 6ES7653-2BB00-0XB5: PCS 7, SOFTWARE, RUNTIME LICENSE AS (PO 1000), FLOATING LICENSE F.1 USER R-SW, WITHOUT SW AND DOCU. LICENSE KEY ON USB STICK, CLASS A, EXECUTABLE UNDER XPPROF REFERENCE HW: PCS 7 547C: ES/OS PCS 7 An error occurs when we are trying to transfer those licenses to the PLC with ALM: Screenshot #1 As far as I understand AS RT PO license which we have is not compatible with that PLC. Anyway that license is present in siemens catalogue in 410-5H section: Screenshot #2 Also that license can be added in TIA Selection Tool. How we can use those licenses for expanding AS PO in our system?
Attachmentimages.zip (287 Downloads) |
Last edited by: Jen_Moderator at: 2/26/2019 8:45:59 AMRemoved links and added files as an attachment. |
|
2/25/2019 12:53 PM | |
Posts: 64 Rating: (7) |
Hi, How are you transferring them? The process object licenses are 'booked' during the compile/download procedure, and not dragged/dropped in the ALM, as you would with other licenses. Here is a link describing the procedure, I hope this can help you towards a solution |
Last edited by: Jen_Moderator at: 2/26/2019 8:59:20 AMOptimized link. |
|
This contribution was helpful to1 thankful Users |
2/25/2019 7:37 PM | |
Joined: 2/1/2010 Last visit: 4/19/2024 Posts: 130 Rating: (66) |
As K2016 said, the AS PO are booked from your ES upon downloading charts, there is nothing to do in ALM with that license. One point to clear up which may be your confusion. There are "multiple kinds" of AS PO for the 410 controller. SE (system expansion) PO and AS RT PO. Your SE limit is 500 and RT PO is 1000 based on the parts you provided. If you have already exceeded your 500 SE PO limit and need to increase (or you just want them to match for future expansion) you can order more using part number 6ES76532CA000XK0 for 100 increments downloadable, or 6ES76532CC000XK0 for a 500 increment. You will need to use ALM to upgrade the AS with the SE PO. I can't find the procedure now, but it is available when you purchase the SE POs. Note you need 1 set for each controller of an H-CPU, so order qty 2x 100 for each increment of 100 or 500. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to4 thankful Users |
2/26/2019 5:15 AM | |
Joined: 11/15/2017 Last visit: 8/13/2023 Posts: 6 Rating: (0) |
thank you all for your support! |
Follow us on