2/15/2020 1:08 PM | |
Posts: 3 Rating: (0) |
can any body help me I am net PLC Programmer when I load program in S7-200 Simulator I get error "The File cannot open to read" I am using V4.0 Step 7 MicroWin SP9 please check error pic also ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/17/2020 06:51:15New subject after splitting |
|
2/17/2020 10:22 AM | |
Posts: 3 Rating: (0) |
I am using PLC S7-200 CN siemence product . when I load the program in the simulator it shows an error which I have already attached. |
2/17/2020 10:51 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
That's not a useful error to analyse the problem. Have you more details ? Regards, Scorp |
2/17/2020 11:35 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
And the simulator is not a Siemens product..... |
Follow us on