Industry Online Support
Technical Forum
7/21/2007 7:01 PM | |
Posts: 3 Rating: (0) |
Yes, the system had been working perfectly until the leaking pipe incident. I don't know how to carry out your suggestions. Can you explain? |
7/23/2007 8:19 AM | |
Posts: 2930 Rating: (432) |
Hi, here is a list of information and so on you get for free from Siemens: (FAQ)http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&caller=view&lang=de&siteid=csius&aktprim=0&extranet=standard&objid=10805149&treeLang=deForumhttp://www.automation.siemens.com/WW/forum/guests/Conference.aspx?ForumID=15&onlyInternet=False&Language=deDownload Demo Softwarehttp://www.automation.siemens.com/_de/s7-200/support/tools_downloads/index.htmlAdditionalSoftware-Downloads (Service-Packs, usw…)http://support.automation.siemens.com/WW/view/de/10805149/133100 Programing Tips http://support.automation.siemens.com/WW/view/de/1232912Web Based Training SIMATIC S7-200 (Online-Training)http://www.sitrain.com/html_00/f_11_simaticwbt.htmlMicro Automation Sets www.siemens.de/microset(unter “Support” kommt man u.A. zu den Startup-Codes für die jeweiligen Sets)Customer magazine“GO!”http://www.automation.siemens.com/magazines/go/html_00/go.htmWith the demo software you have no limitations for 60 days. If you PLC program is password protected then there is no way to "crack" the PW. The only thing you can do is to clear the PLC memora and set the PLC to the factory settings (use the PW: CLEARPLC) if the PW screen appears to do so. I hope this helps. Regards Helmut |