2/9/2015 10:21 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
What's gone wrong with uploading? Power failure? Connection between the PC and logo interrupted? |
2/9/2015 10:49 AM | |
Posts: 11 Rating: (0) |
I cannot connect the 0BA7 anymore - it doesn't stop rebooting (see the video) |
2/9/2015 10:56 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Is there an SD-Card in the logo? |
2/9/2015 10:58 AM | |
Posts: 11 Rating: (0) |
No, I have never used an SD card yet... |
2/9/2015 11:05 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Is not known to me. |
2/9/2015 11:07 AM | |
Posts: 11 Rating: (0) |
Now I think that it might have happened so that I pushed "start" (the PLC program) on both - and PLC (via keypad) and in SoftComfort. |
Follow us on