5/7/2012 6:14 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hello all, my tests with the block "stop watchwatch" of the LOGO!-0BA7 showed following: Have a look at the circuits for this purpose in the file attachment: Test_Stopuhr_02 (0BA7).lsc: show now how with the aid of a block "analogous comparator" at least an advertisementadvertisement-duration of 65 s with a solution of 0,01 s is possible for time format ss:xx0 s by means of a further trick. Test_Stopuhr_03 (0BA7).lsc: Now a DEMO is, as under observation of mine or g. findings a time indication about a maximum duration of 99 h and 59 m with a resolution of 0,01 s can be reached! (Comment: Connects once in the PC_Simulation into the "font 2" of the text message around a suitable date representationdate representation see...) My upshot: Best regards Betel AttachmentDEMO_Stopwatch_03_0BA7.zip (305 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on