11/25/2015 8:39 PM | |
Posts: 16 Rating: (0) |
pls reply |
11/26/2015 8:50 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, you can insert a fuse below 1A, then you can put one of 800mA as the series 477 of the catalog below for example: 5x20mm Fuses - Littelfuse |
11/27/2015 9:45 AM | |
Posts: 16 Rating: (0) |
No no i just want to clear myself should i use the 250 V 750mA fuse i have written before with my 12 V 1A DC adaptor |
11/27/2015 6:00 PM | |
Posts: 16 Rating: (0) |
hi while reading the manual of logo 8 suggested by ixo65 [https://support.industry.siemens.com/cs/document/100761780/logo!?dti=0&lc=en-WW pg-49 ] pls see the attached image ------- i have marked the points below with the same number encircled red, 1. i found i have to connect "Ground" near the RJ45 ethernet port, now my confusion is that I am using a DC power supply with only two pins + and - so should i connect this "Ground" to the - (negative) wire of my supply, clearly i mean that i short this "Ground" and "M' of the logo 8 ------- is it OK 2. the second confusion is that I could not find the current limit of inputs of logo whether i connect fuse (750mA,250 V or what value) to each input I1, I2 ... I8 that i use along with on main supply L+ 3. should i use a fuse for o/p relay contacts for their protection thanks, pls reply soon |
11/28/2015 5:13 PM | |
Posts: 16 Rating: (0) |
pls reply, pls pls |
12/2/2015 6:26 AM | |
Posts: 16 Rating: (0) |
Pls anybody reply the circuit i made is ok and safe or not? pls reply so that i can give a safe 1st start with my logo 8 thanks |
Follow us on