6/25/2010 5:06 PM | |
Posts: 4 Rating: (0) |
derf thanks for being honest. chyde |
6/30/2010 4:03 PM | |
Posts: 167 Rating: (65) |
Hi Logo!Barbarian, i'd like to answer your questions 1) the Excel Logger should work also with modem or GSM connection. The Insys module is working like this. GPRS can cause delay problems because of the ip network,but the timing can be adapted to the delay in VB. 2) You can write your own software and read out the logo data. It's not a mystery to get out data. The first Logger software was running on a DOS PC and the code was written in Turbo Pascal. I've tried a programmable serial-IP converter (www.tibbo.com) to visualize the data on web pages. This is also working. Programming laguage is an object orientated basic dialect. If you are interrested i can put it online again so you can have a look. It should be very easy to translate the excel VB part into any other language. Superbrudi |
This contribution was helpful to1 thankful Users |
7/1/2010 11:15 AM | |
Posts: 21 Rating: (1) |
Hi, i'm interested Rafa |
7/1/2010 8:26 PM | |
Posts: 167 Rating: (65) |
Hi, here is the link to my tibbo device server with a very small Logo! webpage. https://m0007872-p81-h2887095e05fa2cce1a4fb21a0d189d2aa3954417.webdirect.mdex.de Its a temperature control system for my house with a logo switching a fan on and off. It will be online over the weekend. Cheers Carsten |
This contribution was helpful to1 thankful Users |
7/8/2010 12:38 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Hello Holland, i will look into this in the next week. Fred (Derf) |
7/8/2010 8:15 AM | |
Posts: 167 Rating: (65) |
Hi derf, i modified the VB code to save the xls file automatically. You will find this at the end of the german threat /tf/WW/de/Posts/45463 Superbrudi |
This contribution was helpful to2 thankful Users |
7/9/2010 5:45 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
SUPERBRUDI, thank you very much fred (derf) |
5/19/2011 11:18 PM | |
Posts: 2 Rating: (0) |
Hello Superbrudi, Can you tell us, if you have finished your software for communicate with the logo! ? I tried since few days to communicate with it to se the inputs/output and i think we can send some action to the PLC ??? thanks for your help Songotag |
Follow us on