Industry Online Support
Technical Forum
3/6/2014 8:13 AM | |
Posts: 2930 Rating: (432)
|
Hi, to disable the menue for the TD is not possible. When you want to use the F-keys ion your program, then you can create a message two times and change between this two messages very quickly. The result is, that the press of the ESC key (necessary to go to the menue) is not possible any more. You need to set the time where the TD change to the scantime of the program. If you need to use F-keys and Cursor buttons, then it isnopt possible. Here an example: Hope this helps AttachmentLock TD menue.zip (269 Downloads) |
This contribution was helpful to1 thankful Users |
3/6/2014 8:35 AM | |
Posts: 4 Rating: (0) |
hi, thanks very much for the reply and attached example. I will give this a try today. Thank you
|
Follow us on