5/13/2014 9:55 AM | |
Posts: 1299 Rating: (135)
|
Hello, did you configure any system function to change to start screen with user change or similar? K!ke |
5/27/2014 11:21 AM | |
Posts: 1299 Rating: (135)
|
Hello, you are right, you need to use the screen windows for this issue. I think you are talking about this faq (with the autoload.pas) http://support.automation.siemens.com/WW/view/en/16626380 This one is valid for wincc (until v7) and PCS7, not WinCC Professional V11. But still I'm not sure about your problem. you have the screen "screenS" with the two screen windows "screen 1" and "screen 2". If you close the logon dialog it activates the "screenS" which means you see "screen 1" and "screen 2" ? K!ke |
Follow us on