11/30/2021 6:01 AM | |
Joined: 6/30/2015 Last visit: 6/11/2024 Posts: 31 Rating: (0) |
HI experts. I am using tia portal version v15.1 and v16, and even in V16 I am not able to find hardware 6ES7515-2AM02-0AB0 v2.9. I am looking for GSD 6ES7515-2AM02-0AB0 v2.9. In the hardware config v16, it only allows me to install 6ES7515-2AM00-0AB0 6ES7515-2AM01-0AB0(v2.8). with 6ES7515-2AM01-0AB0(v2.8) i am not able to download
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/30/2021 07:57:36New subject after splitting |
|
11/30/2021 6:05 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205) |
For use all functions of the firmware V2.9.x you need TIA V17. There's no GSD for TIA V16.
Attachment6ES75152AM020AB0_datasheet_en.pdf (323 Downloads) |
11/30/2021 6:08 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205) |
See also this product note: New firmware version V2.9 for SIMATIC S7-1500 and ET 200 CPUs |
11/30/2021 6:33 AM | |
Joined: 6/30/2015 Last visit: 6/11/2024 Posts: 31 Rating: (0) |
so there is no chance to download backup in 6es7515-2am02-0ab0 (v2.9). from Tia portal V16. |
11/30/2021 6:51 AM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205) |
You can make a project with TIA V16 with FW 2.8 an upload it to the PLC. This is possible. How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)? |
11/30/2021 7:00 AM | |
Joined: 6/30/2015 Last visit: 6/11/2024 Posts: 31 Rating: (0) |
but when I am downloading I am getting this error(attached picture) and then I am not able to download |
11/30/2021 8:01 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
check diagnostic buffer for error details |
Follow us on