1/21/2020 6:46 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33005 Rating: (4078) |
You're right. Also flag adddresses beginning at Byte 0, Bit 0. So is M0.0 the first bit in M area.
AttachmentBit, Byte, Word and DWord.pdf (257 Downloads) |
This contribution was helpful to1 thankful Users |
1/21/2020 6:55 PM | |
Joined: 2/7/2019 Last visit: 2/22/2024 Posts: 33 Rating: (2) |
So if %M0.0 is the start, how far can I go with %M ? Is there an end address? |
1/21/2020 8:17 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33005 Rating: (4078) |
In the manuals of the CPUs. |
Follow us on