7/11/2019 10:49 AM | |
Joined: 3/30/2015 Last visit: 3/15/2022 Posts: 1 Rating: (0) |
Hi. I have a challenge with one of my Packing Machines. The packing machine runs with Simotion D425 DC drives with the following part numbers and specifications: Smart Line Module -Input:3AC,380-480V, 50Hz -Output: DC 600V,17A,10kW -Part Number: 6SL3130-6AE21-0AA0 SINGLE MOTOR MODULE -Input: DC 600V -Output: 3AC,400V,18A -Part Number: 6SL3120-1TE21-8AA3 DOUBLE MOTOR MODULE -Input: DC 600V -Output: 3AC,400V,3A/3A -Part Number: 6SL3120-2TE13-0AA3 The problem starts when we switch over to the Generator after a power outage. The machine runs for approximately 10 minutes and stops due to “Simotion Error fault”. The following actions were carried out:
The following actions were also carried out:
However these actions did not yield any positive results. Please help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/11/2019 14:31:15New subject after splitting |
|