Industry Online Support
Technical Forum
7/29/2013 1:12 PM | |
Posts: 5 Rating: (0) |
Hi all! I have a project. that is STS crane system for port. My system are 4 motor group. Main Hoist, Trolley, Gantry and Boom.My partner chose transformer for the system. and i have to check. I think some problem. + In crane systemMain motor type choice is continuous S1. But in mechanic calculation the duty is S3. In STS crane, the hoist motor frequently have to increase / decrease speed and braking. I think, when we calculate, we have to calculate is P2=PRMS*1.4. + i don'tknow what the calculations were correct or not? Please help me! Caculation file attached thanks!
Attachmentcaculation trans.pdf (221 Downloads) |
Last edited by: O_Moderator at: 7/29/2013 8:24 PM |
|
7/30/2013 11:19 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is published in the following thread, too. Main transformer capacity calculation for STS Crane system Best regards O_Moderator |
Follow us on