3/22/2012 12:57 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hello. Help me please with the settings needed for monitoring network components. I'm using PCS 7 v7.1 SP3 on IPC547C (with Windows Server 2003). Network configuration is shown in atttachment 1.png. OS Server is also used as MS Server. I've read many documents about this topic, but still have several questions. 1. First of all, do I need to connect CP1623's free port with one of the Ethernet adapter? This manual PCS 7 Network Diagnostics with the SNMP OPC Server says that we shouldn't mix ISO and TCP/IP protocols on the same Plant bus and additional TCP/IP adapter should be used for SNMP. 2. Are the IP addresses assigned correctly? 3. Do I need to configure IE General for Plant bus SNMP in HW Config? And as for SNMP OPC Server configuration: see attachment 2.png (CAS and Client are not present at the moment) 4. Diagnostic hierarchy consists of AS objects, Network objects and PC stations. PC stations have been automatically added to Diagnostic screen and they are monitored via Plant bus (Maintenance shows Address 192.168.2.1x). Nevertheless should I add PC stations to OPC Server and what bus (all three?) to choose? 5. Am I right with selected profiles? In this configuration Export Tags for WinCC function doesn't show any warnings. But, for example, if I'd choose "Profile_Simple_SCALANCE_X208_X208PRO_V1_1.txt" (also the same with other SCALANCE X208 profiles) for SCALANCE_X208 I'd get a warning: The profile does not match the selected device. The profile does not include all required variables. 6. That SCALANCE X204-2 looks very poor in it's Maintenance window. The only 5 not empty fields from 15 are: Comment: some-comment.. Identifier: SCALANCE_X204_A Address: 192.168.2.201 Device type: "ALANCE X204-2, 6GK5 204-2BB10-2AA3, HW:" Last update: some-date.. What can I do with this? How to split Device type information into relevant fields? 7. Do I need to adjust DiagMonitor if PCS7 is used? Local machine is added in DiagMonitor on every IPC – is it enough? Thank you, guys! Attachmentpictures.zip (134 Downloads) |
Last edited by: TerminalBuzz at: 3/23/2012 11:50 AM7th question added Last edited by: O_Moderator at: 3/22/2012 1:18 PMpictures transferred to attachment |
|
3/28/2012 1:39 AM | |
Posts: 2661 Rating: (279)
|
See chapter 15 in the following manualfor which profiles to use: PCS 7 Operator Station (V7.1) For general info see following: |
4/25/2012 11:57 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hello again.
All right, it is working! My problem was that I was told about that strange connection between CP1623 and another Ethernet adapter + that manual told about additional TCP/IP adapter needed, so I agreed. And I assigned IP 192.168.1.2x for free Ethernet adapter, so when you told me that I should use simply CP1623 I tried just to unplug Ethernet cable that was connecting CP and Eth-adapter – and it was a wrong testing approach. And when I had finally disabled Eth-adapter, the NDIS adapter began working. I can also just change IP network identifier from 192.168.1.xx to 192.168.0.xx – ok too. 2. It’s clear now. I disabled so called Plant bus SNMP Eth-adapter and changed its name to “reserved”. I can't see a detailed diagnostic for IPC stations. Simply "online/offline" 5. The community of the IPCs isn’t correct. You selected “public”, but “SOL” is correct (You won’t find it in the drop down menu but you can simply write it into the field). Further, please take only the released and tested profiles for Scalance. Please select the profiles which are named in the following FAQ: http://support.automation.siemens.com/WW/view/en/27833758 So, if you will use a SCALANCE 208 you have to take the profile “SCALANCE X200_V”XX”.txt” The message for “automationManufacturerId,automationFunctionTag” can be ignored because this is a new variable which is available only in the new Scalance and new PCS7 Version. This has no effects on your plant. Good. 6. Please use the correct profile. The profiles which are listed in the documentation are released and tested with PCS7. See attachment. But in WEB Management of that Scalance the Device type field is: SCALANCE X204-2 7. Do I need to adjust DiagMonitor if PCS7 is used? No Does it connected with PCS7 Asset Management? Yes Local machine is added in DiagMonitor on every IPC – is it enough? Yes Should it be started with Windows and could it work as a system Service? Yes, it should be started with Windows and Service is not necessary. If DiagMonitor is launched with Windows it won't hide to System tray despite of the settings of DiagMonitor: 'Start with Windows' and 'Minimize to System tray' I think this is no matter? If yes, we have to open a separate ServiceRequest for our colleagues which are responsible for DiagMonitor. This is not too bad, but I would like DM to hide to system tray automatically. |
This contribution was helpful to3 thankful Users |
5/6/2012 11:16 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
I hope someone is interested in my issues. We had continued to discuss the 4th question: - I checked your screenshot and there are wrong computer names entered. It is very important that the name in the OPC server configuration is exactly the same like the computer name under Windows. In your case the OPC server configuration name is "CWA03_plantbus" . I think the real computer name is "CWA03". So, please name it like that and export the WinCC tags again as well as updating / generating the diagnostic screens again. - By the way, I tried to use “Export CSV” while changing PC name and adding Nodes. But I’ve got an error with “Import CSV” function. Object Properties (4502:1063) Then I opened .csv and leaved just one row of data. And so “Import CSV” function showed no error. But I can’t make Import with one-row-csv several times to fill the Node list, because every Import operation is cleaning the list beforehand. - How can you prevent the creation of two PC stations (ES and MS client) in the process picture of the Maintenance Station when they are configured on the same computer? Nothing new for the 6th question about Device type field. I guess I should correct it with a script, split the data and show just the correct part.. |
Last edited by: TerminalBuzz at: 5/7/2012 10:44 AMadd answer |
|
This contribution was helpful to2 thankful Users |
Follow us on