11/9/2011 10:11 PM | |
Posts: 196 Rating: (12) |
Hi I got at strange problem with the Maintenance Station in PCS7. The Setup is AS system, network 4 client, Engineering station and a redundancy server pair. I have configured the SNMP OPC according to Manuel “PCS 7 Network Diagnostics with the SNMP OPC Server” http://support.automation.siemens.com/WW/view/en/18804292 My client 4 station is working and I have access to PDM configuration and I can get the information from my network. But on client 1,2,3 get no information in the diagnostic area. From the script debugger I get this message “IVar2Control raised an error: “ I have verified that my configuration is the same at my client, so I don’t understand it works on one client and not at the rest. I have attached the log from client 4 and 2, and screen shot. Thanks in advance. AttachmentLog_ScreenDump.zip (66 Downloads) |
Follow us on