11/10/2008 2:20 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
helloEng.Nidaa Making a project asone executable projekt is not possible. What do you want to do? I can imagine. Best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
11/10/2008 2:33 PM | |
Posts: 16 Rating: (0) |
ohhhhhhhhhhhhhhhhhhhhhhhhhh myyyyyyyyyyyyyyyyyyyyyyyy god you kill me with this news thanx any way |
11/10/2008 2:48 PM | |
Posts: 487 Rating: (44) |
what exactly do you need? Are you looking for a project that runs when yourun an exe, or looking for a project installation setup as an exe? |
11/11/2008 1:50 PM | |
Posts: 102 Rating: (11) |
Hi!! If it is about a security issue, you should know you can make the project "Full Size" and disable ALT-TAB functions =) |
11/12/2008 10:17 AM | |
Posts: 16 Rating: (0) |
hello all i'm working on a wincc v6.2 package, i wanna make my project as an EXE file, such i can open it without openninng WINCC explorer.. thanx in advance |
11/13/2008 8:58 AM | |
Posts: 102 Rating: (11) |
Hi! There are different approaches to do this... You can, for example, enable passwords in all the C and VBS functions in the Global Script... you can disable ALT+TAB and make that the project runs in AutoStart so the operator does not have a chance to go out from it... There is a similar thread about this /tf/WW/en/Posts/12118 |
Follow us on