1/13/2009 3:40 PM | |
Posts: 20 Rating: (0) |
Hey i wonder if anyone can help me with this, i use a TC65 modem with a s7-226 cpu and use siemens SET5 https://support.automation.siemens.c...45&caller=view to send SMS and it works as it should, and now i need to send a command so i know if the modem have connection to the network, going to do that every 1minute or so, was asking that to siemens support and the told me this "I’m sorry, we’ve no example for that. You can send “at+creg?” with STR_CPY to VB1796. With a block RCV you can save the answer of the modem to a value . What answers you can get you can find here: http://www.nobbi.com/atgsm.htm#+creg “1” means your modem is logged in. I’m sorry, I only know this German site." and i don't know how to use str_cpy and block rcv, any one that can make me an program exemple? |
Last edited by: O_Moderator at: 4/14/2010 1:00 PMsubject edited |
|
2/23/2009 3:27 PM | |
Posts: 20 Rating: (0) |
I have already change to ver. 1.20 first i deleted the POU in my project and then after that i was building up sms_init, send, receive again. when i right click on library for allocate memory, still version 1.15 is there how to delete a library complete? maybe that is my problem now when i only get 2 on the status word, and then timesout to 21 https://www.automation.siemens.com/tf/WW/en/Posts/26941#124782 but i had problem with sending SMS before also, works sometime and other times not. i have the modem with me home so going to see if i have a PLC so i can get this working |
2/23/2009 11:55 PM | |
Posts: 20 Rating: (0) |
Now i have maked 2 new project, 1. with 1.15 that i downloaded a year ago, and works to send sms 2. ver. 1.2 downloaded here https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=21063345&caller=view and that one doesnt work to init, i only have 1 port on the PLC so i cant look at the status word. why cant i use that lib that is on the page for send sms? going to make a try with 1.16 now.. .................. that one that u linked to is for GPRS stuff? dont know how to use that lib. to send SMS with my modem i use TC65 and only wanna send/receive SMS |
Last edited by: Ason at: 2/24/2009 12:08 AM |
|
2/24/2009 9:47 AM | |
Posts: 20 Rating: (0) |
Sorry, i mean version 2.1 i attached the 2 sample files i did last night, version 1.15 that worked earlier version 2.1 that i cant get to work at all i wanna update the library to the newer one because i have problems to login to the GSM network sometime and wanted to see if it was going better with the new version. i dont have version 1.15 any more in microwin libraries but i have a older version of the project that use it, and also the sample project that i attached now. AttachmentSMS.zip (204 Downloads) |
2/24/2009 2:31 PM | |
Posts: 20 Rating: (0) |
Hey now i also call sms receive and now different, i cant make a good sms_init at the site where i can be online to see what happens it stops on status word 2 echo off found out that i have version 2.0 of the library and that one works good also with my setup, SM_INIT is done in a couple of seconds and also SMS_SEND still i cant understand how to use SINAUT MICRO SC S7-200 Block Library Update V1.16 to send SMS with my TC 65, is that possible? what i have done in my project: 1. used version set5_s7-200-library.mwl version 1.15 worked to send sms, but some time SMS_INIT doesnt work, 2. deleted every POU in my project that is for SMS handle, installed set5_s7-200-library_port0.mwl Version 2.1 and now SMS_INIT doesnt work, now what i think to try to night, deleted every POU in my project that is for SMS handle, in library memory allocation im going to delete library symbols setting up new calls for sms_init,send, receive with version 2.0 in my project, and hope it works. next step is to increase waiting time in block sms_xmt_rcv_manage so it have longer time to login to the GSM network i was told that is in network 10. Attachmentsmstest_V2.1lib.zip (131 Downloads) |
2/24/2009 3:36 PM | |
Posts: 20 Rating: (0) |
When i make a version check with 2.0 it seams to go to make a update but a version check with 2.1 it doesn't looks so i have attached 2 print screens haven't done any update yet, going to try it to night.. Attachmentversioncheck.zip (120 Downloads) |
3/11/2009 9:58 PM | |
Posts: 20 Rating: (0) |
Connected with HyperTerminal to the modem with 9600 speed sending this AT commands: AT+CPIN?$R +CPIN: READY AT+IPR=9600$R ERROR AT+IPR=9600 ERROR ATE0$R ERROR
AttachmentSMS_lib2.0_sms_check.zip (148 Downloads) |
3/11/2009 10:09 PM | |
Posts: 20 Rating: (0) |
Was unpluging the ppi cable and now i got TX/RX flashing, but still no sucess SMS_INIT |
Follow us on