Industry Online Support
Technical Forum
9/30/2008 3:16 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi! Are you sure, that you are using the correct code? (Set5_S7-200_V2D11_en.mwp). You see there the Subroutine "mode_mng". In network 1 you see, that the input E0.5 (en.: I0.5) is used to start the init mode. http://support.automation.siemens.com/WW/view/en/21063345 When you have a look to the OB1 --> Network 4 you see the SMS_init block. Please have a look to the "INIT_status" output-word. Maybe i can give you a hint with this information from you. regards Lif |