6/27/2016 5:25 PM | |
Joined: 5/27/2014 Last visit: 11/3/2023 Posts: 81 Rating: (11) |
Hi, there are two application examples for mass Engineering: |
This contribution was helpful to1 thankful Users |
6/27/2016 8:51 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Guys, I suggest you will not look into Advanced ES. This piece of addon software was introduced with PCS7 v8.0, but is discontinued as of v8.2. It is not supplied anymore with the media package. It was based on COMOS. Siemens is working on a new piece of software I believe, in order to use with Control Module Types, but further information is yet unknown. At this moment, COMOS provides full use with Control Module Types. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
6/28/2016 9:15 AM | |
Joined: 6/14/2006 Last visit: 6/29/2023 Posts: 301 Rating: (60) |
Hi, the successor of Advanced ES is PCS 7 automation base. Find the manual there: https://support.industry.siemens.com/cs/de/de/view/109737945 Regards |
This contribution was helpful to3 thankful Users |
Follow us on