Industry Online Support
Technical Forum
6/2/2010 11:15 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User anshul godikawrote: Hi I am prasoon Please tell me how to Program Master Drive for speed variatin with the joystick on profibus. i.e. my joystick and Master Drive both are Profibus nodes. so through PLC how to program so that when i move my joystick on profibus that speed should vary |
6/2/2010 12:15 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181)
|
Hello, Unfortunately you could n' find project exactly covers your requirements. The idea is - improve both "devices" in Profibus network. Look at http://support.automation.siemens.com/WW/view/en/20386822 There you'll find simple project how to exchange data (control the drive and receive statuses from it) with master CPU. Using the same way and using manual of actual type of drive you could see where you give command to go FWD or REV. Meanwhile you'll read positions of the joystick. Simple just put them in a right place. Give more details about drive and type of joystick. Best regards, Hristo Mihalev |
Follow us on