Industry Online Support
Technical Forum
6/10/2009 9:04 AM | |
Posts: 17 Rating: (0) |
i have s7 400 plc and s7 300 i have to establish the master slave communication |
6/10/2009 10:11 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Salman92. I'm quite sure it has been discussed here many times but anyhow, Check this FAQ. Also check Module D6 in this link. It is the same either the DP-Master is S7-300 or it is S7-400. Best regards. H-H |
6/10/2009 10:49 AM | |
Posts: 557 Rating: (64) |
hi find the link, hope this will help........ http://support.automation.siemens.com/WW/view/en/6518822 regards |
This contribution was helpful to1 thankful Users |
6/15/2009 11:51 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hi Paresh, Look at What differences are there when configuring S7 connections? and What properties, advantages and special features does the S7 protocol offer? Example: How do you configure an S7 connection for data communication between an S7-200 and an S7-300 or S7-400 on the Industrial Ethernet? Regards Hristo Mihalev |
6/15/2009 12:22 PM | |
Posts: 116 Rating: (1) |
Hi Umencho, Thanks for your reply. Regards Paresh |
Follow us on