5/12/2006 9:24 AM | |
Joined: 4/24/2006 Last visit: 10/8/2025 Posts: 9027 Rating:
|
Hi, Perhaps the following link will help you, http://support.automation.siemens.com/WW/view/en/19449428 It's a master - slave configuration, unfortunaly the S7-400 is master and S7-300 is slave. ![]() But I hope it will help you, Wizard |
5/18/2006 3:59 PM | |
Posts: 22 Rating:
|
Hi All AttachmentBel1.zip (1066 Downloads) |
5/18/2006 4:21 PM | |
Posts: 22 Rating:
|
Hi All how can i do hardware configration? how can l perform configuratelikeattached folder and how can ı use sfc14-sfc15. For example ı want to read analog output from slave plc and i wantto write any data block to master plc. Attachment46.zip (1183 Downloads) |
5/18/2006 4:45 PM | |
Joined: 4/24/2006 Last visit: 10/8/2025 Posts: 9027 Rating:
|
Hi, The following link is a manual where SFC14 and SFC15 are explained: http://support.automation.siemens.com/WW/view/en/1214574 In the configuration tab of the S7-318 (slave), you can specify how many byte's or words you want to communicate. Greetings, Wizard |
5/22/2006 9:52 AM | |
Joined: 4/24/2006 Last visit: 10/8/2025 Posts: 9027 Rating:
|
Hi erenakc, When you want to use PUT and GET, you'll have to use FB14 and FB15 in the S7-300. And you'll have to use a CP342-5. See the following link: http://support.automation.siemens.com/WW/view/en/22991863 But with the hardware you've got, you can use SFC14 and SFC15, see the attachment project. ![]() Best regards, Wizard Attachmenttest.zip (1036 Downloads) |
Follow us on