Industry Online Support
Technical Forum
10/21/2011 10:46 AM | |
Posts: 2 Rating: (0) |
I have a problem on a belt conveyor which has 4 masterdrives.Three of them are tripping on F150 at once the master inclusive.Please assist. |
9/29/2018 7:46 AM | |
Posts: 7 Rating: (0) |
Our drive , MLFB# 6SE 7100 - 0ZS92, 1500kw for roller press application , having the fault F150, digital input was high( DI1 at EB1, X48:40), it was auxiliary contact (NC)of control breaker. replaced the breaker, fault disappeared, drive started normally. See the attached file for drawing and input signalAttachmentF150.docx (120 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on