9/12/2012 9:18 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Greeting fbelic, Actually we are using Runtime on Local PC and for Modbus devices we have connected following device server modbus to Ethernet TCP/IP http://www.perle.com/products/IOLAN-SDS-Rack-Terminal-Server.shtml above device server can be communicate 496 modbus devices with WinCC flexible @ different slave address we have no issue on hardware side. [schnippschnapp] Thanks, Regarded. |
Last edited by: O_Moderator at: 9/12/2012 10:47 AMnew question is splittet to /tf/WW/en/Posts/80101#top MS |
|
9/12/2012 10:50 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the following thread WinCC flexible Open Modbus Best regards O_Moderator |