11/2/2017 7:35 PM | |
Posts: 8 Rating: (0) |
Hi, I'm having trouble with my auxiliary components connected to an IOT2020 and I think it may be because an excess of power consumption. I have connected to the IOT an usb wifi adapter (consumption uncertain), a sensor connected to the GPIO that takes at most 0.5W. And a pci SIM adapter with a consumption of 2W max. From theiot2000_operating_instructions_e_en-USI got that the max power consumption (of IoT and peripherals) is 10W. I've checkced and the consumption of the system doesn't exceeds 6W. This takes me to think the problem might be with how the power is distributed inside the IOT. Looking in the same file I've found the chart attached. My question is regarding this chart; the distributions of power showed, are strict? or is it more like a guide of possibles (but not the only) configurations? Any comment will be appreciated and I'll be happy of provide any missing information. Thanks in advance. |
Last edited by: Jen_Moderator at: 11/7/2017 1:23:29 PMInserted right link. |
|
Follow us on