7/30/2019 4:34 PM | |
Joined: 2/8/2018 Last visit: 4/18/2024 Posts: 60 Rating: (2) |
Guys Question about velocity. When I preset to measure velocity with 60 s/1min and 4096 increment per rev. I get strange value which I can not understand and most confusing is when encoder is not rotating at all (it is on the test bank) it shos value any way and after a while it goes to 0. I tested it with incremental encoder and it is the same behavior. Can somebody explain it? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/31/2019 10:06:28New subject after splitting |
|
Follow us on