8/26/2008 12:57 PM | |
Posts: 196 Rating: (12) |
Hi Darius.You said the plc won’t set the bit from, from the variable table. I don’t know your program but. But have you check all the diagnose OB12x and OB8x to see if there is not any old code left the in the blocks. Another thing is the memory clock bit in the HW configuration. But it is only 7 bits, and it doesn’t explain the whole problem.Have you made cross Ref. at your program, is a fast way to see what part of your program that is writing to m bit array. As you also describe you have only make a memory reset. Have attached a PDF document that describe, how to format the memory card and how to set the cpu into delivery state again. // Bedst reagard Søren C. AttachmentResetCPU.pdf (258 Downloads) |
This contribution was helpful to1 thankful Users |
8/26/2008 5:20 PM | |
Posts: 196 Rating: (12) |
HI Darius I can understand your a little confused af abut the memory concept,As written earlier you can format the men card by using the MRES,should be able to see a "clean" card.But as you can see there is many ways to format the card.I have attached a link where you can see how the memory concept is build up on pc. http://support.automation.siemens.com/WW/view/en/22605763. |
Follow us on