5/18/2020 10:20 PM | |
Joined: 2/5/2013 Last visit: 4/25/2024 Posts: 320 Rating: (74) |
Hi Habeib_nader My suggestion is better to resolve issue of current CPU otherwise it will create same issue with next CPU also. Which type of error it is showing when you trying to connect It. First you need to check it from which TIA version program is downloaded if Installed TIA and downloaded TIA program is from different TIA platform then you cant upload or download program changes you need same TIA portal. second you need to check whether PLC and PC is in same sub net with different IP address Open TIA Portal In Project View 1.Online access 2.Select Particular driver 3.Update accessible Devices 4.Select Controller ->Online & diagnostics option 5.Diagnostics->Version of TIA Portal Project Please attach these screen shot for 1.Diagnostics buffer 2.Downloaded Version of TIA Portal Project in PLC 3.Installed Software version on PC 4.CPU and Version 5.Error message Br, AmolG |
Last edited by: AmolG at: 05/18/2020 22:22:15Please rate it. |
|
5/18/2020 10:33 PM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4455 Rating: (931) |
@AmolG: @Habeib: Best to have a look at the manual for a full description. |
Last edited by: qwazee at: 05/19/2020 09:32:32The link provided by AmolG works now. Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
5/18/2020 10:45 PM | |
Joined: 2/10/2016 Last visit: 3/26/2024 Posts: 112 Rating: (0) |
Hi Qwazee Thanks alot, but I mean to transfer program from plc to memory card without using TIA Portal |
5/18/2020 10:51 PM | |
Joined: 2/5/2013 Last visit: 4/25/2024 Posts: 320 Rating: (74) |
Hi, Please read link shared by Qwazee or me.It will give you better Idea. First follow suggestion suggested by Qwazee. Power Up and Restart your PLC and PC System. BR, Amol |
Please rate it. |
|
This contribution was helpful to1 thankful Users |
Follow us on