Industry Online Support
Technical Forum
6/5/2008 2:03 PM | |
Posts: 487 Rating: (36) |
Hi Got problem with a script in wincc V6.2 .In the taskmanager the gscrt.exe keeps getting bigger it starts of at about 15K Mem + 15K VMsize and keeps climbing to nearly 1G Mem and 1G VMsize My knowledge of VB script is close to zero , I presume that I have to release something but what and how .... below is a portion of the two scripts used ( global script , every second) hope somebody has some idea Eric Attachmentwinccscript.zip (67 Downloads) |
6/6/2008 1:11 PM | |
Posts: 125 Rating: (26) |
Hi, your script is running on my system. Is "etc" a call of another function or deleted source code? --> use for all objects at the end of your script the call: set <object> = Nothing but i think that will not resolve your problems. If you have further c-scripts with "malloc / sysmalloc", then check if the memory is getting free with "free / sysfree" http://support.automation.siemens.com/WW/view/en/22727197 see this informations for diagnosing errors http://support.automation.siemens.com/WW/view/en/22892165 regards |
Follow us on