4/21/2016 11:59 AM | |
Joined: 1/18/2008 Last visit: 3/20/2024 Posts: 36 Rating: (0) |
In the hardware config for the CPU315-2 DP, are the DB's defined in the Retentive Memory tab? |
4/22/2016 4:15 AM | |
Posts: 12 Rating: (0) |
Retentive MB0 - MB100 and C0 - C6 |
4/22/2016 10:38 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, pls look at this info: |
With best regards... |
|
4/22/2016 10:46 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, no setting can help you to prevent such error. event 9 tells us that the CPU goes in STOP because of memory manegment. So you lost the actual values because of an internal error of the CPU. Your Firmware is very old. Try to update it. Many improvements related to memory loss have been made between FW 3.0.3 and actual FW 3.3.11 Here´s a link to the FW-Download and description how to update it: Operating System Updates for CPU 315-2DP (6ES7315-2AH14-0AB0) hope this helps, regards, |
FCK WAR! |
|
4/23/2016 1:56 PM |
|
Joined: 10/2/2013 Last visit: 4/15/2024 Posts: 339 Rating: (52) |
auto guy is right , i think user automation you should contact to simens support https://support.industry.siemens.com/my/WW/en/requests#createRequest |
Technology is best when it brings people together,so we are here now :) |
|
Follow us on