12/20/2009 9:40 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hello, First of all Step-7 Micro/Win is not compatible with Windows 7. Check here As I know no Siemens software is compatible with Windows 7. Normally when you upgrade Step-7 Micro/Win with an SP you need to run installation of SP and then follow instructions. If it asks to uninstall previous version then you just do so. But never first uninstall previous version before you run SP installation. First you should be asked to do so. Anyway you can do it only on supported operating systems. |
Best regards, |
|
1/20/2010 1:22 PM | |
Posts: 1 Rating: (0) |
hi there i had the same issue, how ever i got it working by using Windows XP Mode. my current PC did not support Virtual PC so i was unable to use XP Mode. However I read VMLite can also run the XP Mode image and is free. I have just tested the VMLite with my XP Mode image and it ran's fine, I have installed STEP7 MicroWin with no issues and uploaded/ downloaded projects to S7-200 PLCs no problems. You can get VMLite from:http://www.vmlite.comjust need to register and download its free. The XP Mode Image you can need to get that first and install from here:http://www.microsoft.com/windows/virtual-pc/download.aspx hope that helps Abdul |
2/2/2010 11:42 PM | |
Posts: 16 Rating: (0) |
I dual boot Vista. Really s*cked to have to do that but I wasn't giving up this new computer to a mechanic.. LOL |
5/6/2011 12:30 PM | |
Posts: 34 Rating: (0) |
C'mon Siemens, its about time you caught up with Microsoft, its now 2011 and you only support an old versions of Windows??? |
5/7/2011 11:56 PM | |
Joined: 8/25/2005 Last visit: 3/21/2024 Posts: 1161 Rating: (110) |
quoting Helmut_13:
I found this reply within the thread Download Software Good luck Sabine |
5/9/2011 11:24 AM | |
Posts: 154 Rating: (17)
|
I have ask the customer support and they tell me thata compatible version for windows 7 is planned for summer this year. |
8/30/2012 11:06 AM | |
Joined: 8/30/2012 Last visit: 12/15/2023 Posts: 4 Rating: (0) |
Hello macbe, could you please explain a little more in detail ? Thanks ! |
10/4/2012 7:25 AM | |
Posts: 22 Rating: (1) |
You need to Run first The MicroWin V3.2, and then installation will not complete-there will be some files missing (for windows 7), dont cancel the installtion. Then you need to have SP9 updates. Then Run the Sp9 updates. The SP9 will successfully install. Worked in Windows 7 (Ultimate and Professional). The Library issue when you press F1, follow the microsoft link for the missing File. Dont download the file from microsoft but copy the name of the file (Windows6.1-KB917607-x86) and search it on Google( Also attached) and download it easily without not having to go a long way with microsoft windows genuine validation. Run the software file and you will be up running with Help library functioning Well and at the End have both MicroWin V3.2 and V4.0. Hope that help. Regards. AttachmentWindows6.1-KB917607-x86.zip (195 Downloads) |
10/13/2012 10:14 AM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating: (1) |
I think MicroWin SP9 supports Windows 7.. Check it out. |
Follow us on