5/6/2011 12:30 PM | |
Posts: 34 Rating:
|
|
5/7/2011 11:56 PM | |
Joined: 8/25/2005 Last visit: 2/16/2021 Posts: 1158 Rating:
|
quoting Helmut_13:
I found this reply within the thread Download Software Good luck Sabine |
5/9/2011 11:24 AM | |
Posts: 154 Rating:
|
I have ask the customer support and they tell me thata compatible version for windows 7 is planned for summer this year. |
8/30/2012 11:06 AM | |
Joined: 8/30/2012 Last visit: 1/12/2021 Posts: 4 Rating:
|
Hello macbe, could you please explain a little more in detail ? Thanks ! |
10/4/2012 7:25 AM | |
Posts: 22 Rating:
|
You need to Run first The MicroWin V3.2, and then installation will not complete-there will be some files missing (for windows 7), dont cancel the installtion. Then you need to have SP9 updates. Then Run the Sp9 updates. The SP9 will successfully install. Worked in Windows 7 (Ultimate and Professional). The Library issue when you press F1, follow the microsoft link for the missing File. Dont download the file from microsoft but copy the name of the file (Windows6.1-KB917607-x86) and search it on Google( Also attached) and download it easily without not having to go a long way with microsoft windows genuine validation. Run the software file and you will be up running with Help library functioning Well and at the End have both MicroWin V3.2 and V4.0. Hope that help. Regards. AttachmentWindows6.1-KB917607-x86.zip (100 Downloads) |
10/13/2012 10:14 AM | |
Joined: 10/24/2011 Last visit: 1/9/2021 Posts: 244 Rating:
|
I think MicroWin SP9 supports Windows 7.. Check it out. |
Follow us on