2/18/2021 10:56 AM | |
Joined: 3/27/2008 Last visit: 4/25/2024 Posts: 1098 Rating: (137) |
Hi Without the keypad resetting the parameters is not possible. If you can find a keypad do the following. Set the following: P0010 = 30 P0970 = 1 Press P DIP switches: Dip 1 is not used, and must be set in the lower position. Dip 2 is for 50/60Hz, for 50 Hz set in the lower position. Software: STARTER, download this: SINAMICS MICROMASTER STARTER - ID: 26233208 - Industry Support Siemens Tractor |
Last edited by: Tractor at: 02/18/2021 11:47:28Last edited by: Jen_Moderator at: 02/18/2021 13:16:09Optimized link. Tractor |
|
Follow us on