8/6/2014 6:22 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello C4ssius, And for information the Led on the Profibus module what color is it?
|
8/6/2014 11:50 PM | |
Joined: 8/6/2014 Last visit: 12/13/2023 Posts: 8 Rating: (0) |
Yeah it is green when I start it up then it changes to red and stops the drive and plc comes up with bus failure. Thanks
|
8/7/2014 8:20 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello C4ssius, Go to chapter 7: Operating Instructions: MICROMASTER PROFIBUS Optional Board Try to open the diagnostic buffer of the CPU for more information MICROMASTER 4 (MM4): What is important when setting up an MM4 with a Profibus module? And follow 2nd post of GDC: MM4V V2.2 DATABAS UPDATE |
Last edited by: Ste39 at: 8/7/2014 8:26 AMAdd Thread From V2.1 to V2.2 Last edited by: Ste39 at: 8/7/2014 8:22 AMAdd FAQ |
|
Follow us on