Industry Online Support
Technical Forum
10/19/2012 8:12 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324)
|
Hi, please see the attachment, it describes the fault, and also on page 2 is the instruction for removing the I/O module. With the power off, remove the I/O module and double check the connections on the back, sometimes the pins can be bent if it was not inserted straight or with too much force. Simply re-seating the I/O module may solve your problem. It sounds like if the drive runs and suddenly stops, maybe there is just a loose fitting of the I/O module. If this does not work, then as a check, you can swap the I/Omodules between drives (just make sure the cables are inserted into the correct terminals. Regards, Graeme
AttachmentFault_and_Instruction.pdf (318 Downloads) |
This contribution was helpful to2 thankful Users |
10/21/2012 10:43 PM | |
Joined: 10/10/2010 Last visit: 9/14/2024 Posts: 307 Rating: (15) |
that's right as i faced such a problem before where my i/o card had one pin broken |
Follow us on