10/9/2016 8:36 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Kal.A, It is OK. i.e. even if you disconnect terminal 5 or 7, the motor will rotate at lower speed. Because terminal 5 & 7 are DI for selection of fixed frequency set point in your case. Fixed frequency setting depends upon the selection of DI1 to DI6. Depending upon the selection of these DI & parameter setting, different motor RPM speeds can be achieved. The control of these DI is must be defined in PLC logic & via HMI or selection operator or system process can control the speed of motor via drive. Please download & refer the Micromaster Vector MMV25 manual here. Operating Instructions: MICROMASTER Vector MIDIMASTER Vector |