Industry Online Support
Technical Forum
3/10/2008 2:10 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, which signals you need depends on application, the simpliest way using PLC I/Os are digital signals run, fault eventually remote ctrl and command run with analog signal/request about speed. Digital signals are 24 VDC, analog output from MM4 is 0-20 mA, inputs +-10 V/0-10 V/0-20 mA. Better way is to use Profibus connection. More info you can find in Operating instructions manualhere: http://support.automation.siemens.com/WW/view/en/24294529 |
Last edited by: Sydney at: 10.03.2008 14:11 |
|
Follow us on