6/10/2016 1:10 PM | |
Joined: 2/23/2016 Last visit: 9/17/2024 Posts: 36 Rating: (2) |
Hello i have a problem with micromaster440 in profibus DP network on the PCS7. when i insert a mm440 in profibus line it's located in bus.but a mini triangle created on mm4's right down. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/10/2016 3:39:28 PMNew subject after splitting |
|
6/10/2016 4:41 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hello Moji, The red triangle means two things: - A GSD file is installed by additional software like DriveES - The drive configured is implemented in your s7/PCS7 project Just an indication.... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
6/10/2016 11:53 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Good evening, I did not know you received an error. It looks you have to update the DriveEs library. You are using v6.1, but you have AP library v8.0 and more installed, so it looks you have an old drive es library. You will have to update those blocks in order to work with PCS7 v8.0 |
If I could help you, you can use the RATE button. Thank you. |
|
6/12/2016 7:23 AM | |
Joined: 11/29/2011 Last visit: 8/19/2024 Posts: 1359 Rating: (232) |
Hi, |
- What you read here, please check with manuals and your requirements. |
|
6/12/2016 6:26 PM | |
Joined: 6/23/2008 Last visit: 9/18/2024 Posts: 1168 Rating: (282)
|
Hello mojtaba.f,
Best regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
Follow us on