10/11/2006 11:58 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
The value you type in is passed into the script as the final parameter, named "value". Attachmentinput fields.zip (292 Downloads) |
10/11/2006 12:09 PM | |
Joined: 8/10/2006 Last visit: 7/15/2024 Posts: 156 Rating: (3) |
Thanks alot, this solves the issue! |
10/11/2006 12:14 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
Glad to help [:D][:D][:D] |
10/11/2006 3:01 PM | |
Joined: 5/19/2006 Last visit: 9/16/2024 Posts: 549 Rating: (107)
|
Now since everybody is up to speed with how an I/O Field updates its OutputValuewould you give it a try with my quiz part 2 (S7 Parser)? This is all about verifying the input data, modifying and return it back into OutputValue. The rules are: check for S7 Address syntax; If the syntax is correct then convert to upper cases, remove extraneous spaces andleading 0s (if any) and write back to OutputValue. If the syntax is wrong don't changeanything just modify the FontColor(red) and write a tool-tip with an error message (see attachment in the post) [:P] Dec |
Last edited by: Dec at: 10/11/2006 3:15 PM |
|
Follow us on